IAR EWB - DMA Driver is not ready and excluded from the build

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IAR EWB - DMA Driver is not ready and excluded from the build

733 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JaiKumar on Thu Feb 18 00:33:53 MST 2016
Hi,

I get this warning message when i try to build for LPC11U67 Microcontroller. I am using IAR Embedded workbench 7.40.
Any  help would be great.

Warning[Pe1105]: #warning directive: "DMA driver is not ready and is excluded from the build"

and in the file dma_11u6x.c file

#if 1
#warning "DMA driver is not ready and is excluded from the build"
#else

does that mean that DMA driver is not written.

Thanks and Regards,
Jai.
标签 (1)
0 项奖励
回复
0 回复数