I2C protocol in lpc4330

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2C protocol in lpc4330

1,433件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by siva4PM on Wed Jun 25 23:16:53 MST 2014
Hi guys,
  In lpc4330 platform, im writing a I2C driver. In I2C base address there is a register called CONSET register which contains I2EN bit, which is for enabling the I2C interface.

My doubt is enabling I2C interface means whether enabling I2C hardware protocol or not?


Thanks in advance.

Regards
siva
ラベル(1)
0 件の賞賛
返信
1 返信

1,311件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Thu Jul 03 11:33:23 MST 2014
Hi,

Yes,setting this bit will enable the I2C hardware interface.

Thanks,

NXP Technical Support
0 件の賞賛
返信