I2C Communication

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I2C Communication

1,183 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by imroun1992 on Fri Sep 13 12:58:06 MST 2013
Hello,

I work on a quadrirotor project which consist to establish an I2C Communication between MCB 4357 Development Kit (LPC 4357) and MPU 6050 Accelerometer. I can't establish this communication, anyone to help me please. Can anyone write a source code for establish this communication and initializing all axis of accelerometer

Thank You
标签 (1)
0 项奖励
回复
3 回复数

1,125 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by imroun1992 on Wed Sep 18 14:29:39 MST 2013
Hello,

I put the datasheet now, can you help how to establish the I2C Communication between KEIL MCB 4357 and MPU 6050 accelerometer. I wan if it's possible a source code to initializing I2C Communication between these component and a code for initializing all axis of accelerometer.


http://dlnmh9ip6v2uc.cloudfront.net/datasheets/Components/General%20IC/PS-MPU-6000A.pdf

Thanks You
0 项奖励
回复

1,125 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Fri Sep 13 14:38:11 MST 2013
I am not familiar with the MPU 6050 acceleromter, but you should be able to use the example code found at:
http://www.lpcware.com/content/nxpfile/lpc4350apdlzip
You can find I2C code in the download.
0 项奖励
回复

1,125 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by imroun1992 on Fri Sep 13 13:04:48 MST 2013

Quote: imroun1992
Hello,

I work on a quadrirotor project which consist to establish an I2C Communication between MCB 4357 Development Kit (LPC 4357) and MPU 6050 Accelerometer. I can't establish this communication, anyone to help me please. Can anyone write a source code for establish this communication and initializing all axis of accelerometer

Thank You



I use KEIL MCB 4357 Evaluation Board
0 项奖励
回复