I2C 5V Toterant

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I2C 5V Toterant

跳至解决方案
1,187 次查看
przemekmaslowsk
Contributor I

Good morning, I would like to ask if the "PIO0_4 / SCL" and "PIO0_5 / SDA" pins in I2C configuration of the microprocessor LPC1313FBD48/01 are 5V tolerant. Thanks so much

标签 (1)
1 解答
1,000 次查看
soledad
NXP Employee
NXP Employee

Hi,

 Yes, they are 5 V tolerant.


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,001 次查看
soledad
NXP Employee
NXP Employee

Hi,

 Yes, they are 5 V tolerant.


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------