How to use both of I2C and SPI in LPC54101

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use both of I2C and SPI in LPC54101

1,323 次查看
takafumisugimot
Contributor I

Hi

I would like to use both of the I2C and the SPI on LPC54101.
However, happen an error on use SPI when I2C was initialized.
Do you know the measures?

When you use this code

ROM_I2CS_Init(devMemI2C, &i2csInit);

mXfer.status is ERR_SPI_BASE on endress.

ROM_SPIM_Transfer(spimHandle, &mXfer);

while (mXfer.status == ERR_SPI_BUSY) {}

This is code

SystemCoreClockUpdate();

Init_SPI_PinMux();

Init_I2C_PinMux();

Chip_Clock_EnablePeriphClock(LPC_SPIM_CLOCK);

Chip_SYSCON_PeriphReset(LPC_SPIM_RESET);

Chip_Clock_EnablePeriphClock(LPC_I2CS_CLOCK);

Chip_SYSCON_PeriphReset(LPC_I2CS_RESET);

Board_Init();

...

spimHandle = ROM_SPIM_Init(devMem, &spimInit);

if (ROM_SPIM_SetupTransfer(spimHandle, &spimConfig) != LPC_OK) {

}

NVIC_EnableIRQ(LPC_SPIIRQNUM);

...

i2csHandle = ROM_I2CS_Init(devMemI2C, &i2csInit);   // If this line does not exists, program will not happen error.

ROM_I2CS_SetupSlave(i2csHandle, &slaveSetup); // If does not exists it, you should comment out of this line

...

optimalDevI2C = Chip_Clock_GetAsyncSyscon_ClockRate() / 4000000;

LPC_I2C_PORT->CLKDIV = optimalDevI2C;

...

NVIC_EnableIRQ(LPC_I2CS_INT);

2 回复数

1,196 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Takafumi,

I Would recommend you to replace the functionality provided by ROM drivers with the LPCOpen API's, this is due to complications associated with ROM based peripheral drivers:

http://cache.nxp.com/files/microcontrollers/doc/support_info/lpc5410x-ROM-Deprecation_1.pdf 

You can download the latest LPCOpen package for the LPC5410x devices on the following link:

LPCOpen Software for LPC5410X|NXP 


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

1,196 次查看
takafumisugimot
Contributor I

Hi Carlos,

Thanks!

I was used the Legacy LPCOpen 2.xx software package.

Best Regards,

Takafumi Sugimoto