How to identify the Date code/year of manufacture of LPC1788FBD208

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to identify the Date code/year of manufacture of LPC1788FBD208

12,925 Views
jayanthyms_bgp
Contributor I

I have procured 25 numbers of LPC1788FBD208 on which the following markings are there:

LPC1788FBD208

SKP483.1

ZSD1821E

Labels (1)
0 Kudos
Reply
3 Replies

1,988 Views
irisA
Contributor I

can you please also help me do decode the date code in MC908QB8MDTE?

top marking is:

MQB8

MDTE

4YYW

thank you 

0 Kudos
Reply

11,970 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello jayanthy M.S. ,

Thanks for contacting our technical support, I will serve for you.

From the marking of your chip, the year of the device was manufactured is the Week 21 of 2018.

It seems this data sheet lost the Marking part, so please have a look at the Errata sheet, in Part I Product identification:

pastedImage_23.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

11,971 Views
jayanthyms_bgp
Contributor I

Hello Alice_Yang,

Thanks for the information.

With Best Regards,

Jayanthy M.S.

On Mon, 18 Feb 2019 04:23:00 +0000 (UTC), Alice_Yang wrote

NXP Community

Re: How to identify the Date code/year of manufacture of LPC1788FBD208

reply from Alice_Yang in LPC Microcontrollers - View the full discussion

0 Kudos
Reply