How to flash image on Custom board lpc54618?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to flash image on Custom board lpc54618?

1,253 次查看
subodhmankar
Contributor II

Hi,

I am able to use lpclink2 to debug my custom board.

But when I try to flash image using lpclink2, MCUXPRESSO IDE shows success but custom board doesn't get flashed.

What are the steps, tools and procedure I should follow to flash LPC54618 custom board?

Please provide me suggested links pr tools...

标记 (4)
0 项奖励
回复
1 回复

1,076 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Subodh Mankar,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
1. Firstly, you should use the correct demo for testing, you can build a SDK for LPC54618 via the following link:
2. Secondly, compare with the OM13092 to check the hardware circuit of LPC54618 custom board.

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------