How to connect 3.2" display to 1769

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to connect 3.2" display to 1769

795件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by p4dman on Mon Feb 02 05:35:39 MST 2015
Hi,
i have this Sainsmart TFT320_QVT display module with a SSD1289 controller:
http://www.sainsmart.com/sainsmart-3-2-tft-lcd-display-touch-panel-pcb-adapter-sd-slot-for-arduino-2...

Additionally i found this article:
http://www.sainsmart.com/zen/documents/20-011-918/3.2LCD+UNO.pdf

In that article i found the pinout of the display module.
Can i connect that wires to any Port of the 1769?
Also i ask myself if i can use the UTFT library which was used in that article on the LPCXpresso. And if i use that library, is it then necessary to have a specific wiring?

Can you recommend any display driver?

ラベル(1)
0 件の賞賛
返信
1 返信

769件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Mon Feb 09 16:06:56 MST 2015
Hi, p4dman,
You can use any port, but make sure your data bus and address bus are each on a single port.
regards,
0 件の賞賛
返信