How to configure the LPC802 to oscillate at the maximum frequency of 15MHz?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to configure the LPC802 to oscillate at the maximum frequency of 15MHz?

847 次查看
leonardobarbosa
Contributor I

Hi everyone!

I am developing a project with the LPC802 and would like to know how to configure the inner crystal to oscillate at 15MHz. From what I understand the FRO must be set to use the 30MHz and then divided by 2 to result in 15MHz. Reading the manual of the item I saw that it is possible to do this using an API that is in the ROM, but I did not succeed, could you help me?

pastedImage_1.png

标签 (2)
0 项奖励
回复
1 回复

703 次查看
jeremyzhou
NXP Employee
NXP Employee
Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to refer to the demos in code bundle, in the demos, it illustrates the way of configuring a system clock frequency of 15 MHz.

Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复