How to Flash a .bin file in a LPC822M101JHI33 if I have a Red Probe+ and a ULINKpro D to interface with SWD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to Flash a .bin file in a LPC822M101JHI33 if I have a Red Probe+ and a ULINKpro D to interface with SWD

935 Views
angelobucciero
Contributor I

I guess I am asking is there a software that can take a .bin file and using the Red Probe+ or ULINKpro D allows me to place it at a given address in the LPC822M101JHI33's internal flash.

If not what to I need?

Thank you

Tags (3)
0 Kudos
1 Reply

494 Views
lpcxpresso_supp
NXP Employee
NXP Employee

You can certainly use the Red Probe+ to connect to an LPC822 with the LPCXpresso IDE : http://www.nxp.com/lpcxpresso

The IDE comes with tools that allow you to program the flash on your LPC822 via this probe, though you might also want to consider an LPC-Link2|NXP 

The following FAQs may be useful:

Using the GUI flash programming tool 

Using the command line flash programming tool 

Red Probe+ support 

https://community.nxp.com/message/630901 

Regards,

LPCXpresso Support

0 Kudos