How do you sucessfully rebulid Blinky (LPCXpresso55S69) example on Arm KEIL MDK?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do you sucessfully rebulid Blinky (LPCXpresso55S69) example on Arm KEIL MDK?

933 Views
AquaSound
Contributor I

Hello community,
I can't rebuild the Blinky (LPCXpresso55S69) example on Arm KEIL MDK.

This example is included in the NXP::LPCXpresso55S69_BSP.
Of course, I also have DFP installed.

*****************************
NXP::LPC55S69_DFP
version 12.4.0 (2021-01-14)

NXP::LPCXpresso
version 12.4.0 (2021-01-14)

ARM::CMSIS
version 5.7.0(2020-04-09)
*****************************

Also, there is a problem with the Run-Time Environment settings of this example project file.

NXP::Device:Startup software components requied NXP::Device:CMSIS:LPC55S69_system.
However, The NXP::Device:CMSIS:LPC55S69_system are not selected.

This issue can be easily fixed from the "Manage Run-Time Environment".
All you have to do is click the resolve button and OK button.
However, even with this fix, the rebuild does not succeed.

The following is the error message when rebuilding.

Build Output:
startup_LPC55S69_cm33_core0.S: Error: A1067E: Output file specified as 'C:\Users\USER_NAME\AppData\Local\Arm\Packs\NXP\LPC55S69_DFP\12.4.0\arm\startup_LPC55S69_cm33_core0.S', but it has already been specified as '.\objects\startup_lpc55s69_cm33_core0.o'
startup_LPC55S69_cm33_core0.S: error: A1023E: File "assembler-with-cpp" could not be opened: No such file or directory

Any clarification would be appreciated.

Thanks!

Labels (1)
0 Kudos
3 Replies

922 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

There is demo for LPCXpresso55s69 under MCUXpresso SDK, it support KEIL, just download and 

open to build:

https://mcuxpresso.nxp.com/en/select  

Alice_Yang_0-1611817324417.png

 

Regards,

Alice

0 Kudos

915 Views
AquaSound
Contributor I

Hello,
Thank you Alice-san,
Your advice is correct.

However, Arm Keil MDK tool customers first use BSP, which can be downloaded from the page at the URL below.

https://www.keil.com/boards2/nxp/lpcxpresso55s69/#/third-party-download-dialog


I want to update this BSP file.
Because, Blinky is also a popular example program on Arm tool-chain.
I think that the fact that the project file can be easily built will lead to the purchase of the device.

Best regards

0 Kudos

888 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello, I test it on my side, it work well

Alice_Yang_0-1613703768540.png

 

It seems you missing a BSP for LPCxpresso55s69 board:

Alice_Yang_2-1613703850632.png

 

Regards,

Alice

 

 

 

 

Tags (1)
0 Kudos