How about 32khz FRO accuracy of LPC8N04?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How about 32khz FRO accuracy of LPC8N04?

958 次查看
li-chinwang
Contributor II

LPC8N04  8Mhz FRO  is 2 % accuracy from LPC8N04 spec following.

How about 32khz FRO accuracy? I can't find it in the spec.

 

 Clock generation  8 MHz internal RC oscillator, trimmed to 2 % accuracy, which is used for the system clock  Timer oscillator operating at 32 kHz linked to the RTC timer unit

标签 (1)
0 项奖励
回复
1 回复

815 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Li-Chin, 

We do not have a characterized number, but the accuracy should not be a problem it would be less than 2%

Hope it helps! 

Victor.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复