Hi NXP team, I want to know how to configured joysticks pin as an external interrupt and how to write external interrupt handler service in general

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hi NXP team, I want to know how to configured joysticks pin as an external interrupt and how to write external interrupt handler service in general

1,214 次查看
oam6
Contributor I

I am designing password based door lock system using LPC 1769. I have build up the code of changing the state but now I am stuck to use joystick pins or switch key 3 or switch key 4 pins to use as an external interrupt. This I am using to reset the system whenever i give an external interrupt. Please help me to configured any switch key to use as an external interrupt and please tell about external interrupt service handler framework in general.  

Your help will be very much appreciated.

标签 (1)
标记 (2)
0 项奖励
回复
2 回复数

1,097 次查看
gc986
Contributor I

Hi!
I'm not going to create a new question, I will write here.
I've created code that should respond to an external interrupt, but nothing happens. In the main cycle, the led flashes (using the open 1788 Board). What is the error, why the interrupt does not work?


#include <LPC177x_8x.H>
#include "lpc177x_8x_gpio.h"
#include "lpc177x_8x_clkpwr.h"
#include "bsp.h"

/* SysTick Counter */
volatile unsigned long SysTickCnt;

void Delay (unsigned long tick)
{
    /*unsigned long systickcnt;

    systickcnt = SysTickCnt;
    while ((SysTickCnt - systickcnt) < tick);*/
    unsigned int i;
    unsigned int i2;
    for(i2=0;i2<tick;i2++)
        for(i=0;i<0x100000;i++){}
}

void EINT0_IRQHandler(void){
    if(GPIO_GetIntStatus(2,22,1)){
        GPIO_ClearInt(2, (1<<22));
        
        GPIO_SetValue(1, (1<<14));
        Delay(500);
    }
}

void SysTick_Handler (void)
{
    SysTickCnt++;
}

void gpio_config(){
    GPIO_SetDir(1, (1<<14), GPIO_DIRECTION_OUTPUT); // LED
    GPIO_SetDir(2, (1<<22), GPIO_DIRECTION_INPUT); // Key 2
}

void setupExtI(){
    NVIC_SetPriority(EINT0_IRQn, 1);
    GPIO_IntCmd(2, (1<<22), 1);
    NVIC_ClearPendingIRQ(EINT0_IRQn);
    NVIC_EnableIRQ(EINT0_IRQn);
}

int main(void)
{
    uint32_t cclk = CLKPWR_GetCLK(CLKPWR_CLKTYPE_CPU);
    /* Generate interrupt each 1 ms   */
    //SysTick_Config(cclk/1000 - 1);
    gpio_config();
    setupExtI();

    //__enable_irq(); // Enable global interrupt
    
    while(1){
        GPIO_SetValue(1, (1<<14));
        Delay(10);
        GPIO_ClearValue(1, (1<<14));
        Delay(10);
    }
    
    return 0;
}

0 项奖励
回复

1,097 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Omkar Mugdar

Thanks for your reply.
To utilizing the external interrupt, I'd highly recommend you to refer to the periph_pinint demo in the LPCOpen library, and you can download the library via the following link:
https://www.nxp.com/support/developer-resources/software-development-tools/lpc-developer-resources-/...
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复