Hardware IP checksum feature removed from ethernet block

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hardware IP checksum feature removed from ethernet block

999件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Johnny D on Wed Mar 19 04:23:05 MST 2014
Hi,

I was wondering if someone could explain this little line in the 43xx user manual?:
"Hardware IP checksum feature removed from ethernet block".

On all the (current) NXP web pages relating to the 43xx mcus, they state "10/100 Ethernet with hardware enabled TCP/IP checksum calculation". But they seem to have removed this feature.

So, will a 4357 do tcp/ip checksum calculations in hardware or not?

Many thanks,

John.
ラベル(1)
0 件の賞賛
返信
1 返信

962件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MarcVonWindscooting on Wed Mar 19 08:52:19 MST 2014
I don't understand. TCP/IP is a protocol on top of Ethernet.
How can the Ethernet hardware know about the TCP payload checksum (without having to know pretty much about TCP)?
0 件の賞賛
返信