Hardfault Handler in LPC55S69

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hardfault Handler in LPC55S69

Jump to solution
3,610 Views
sushmasan
Contributor II

Hello Team,

This is regarding a Hardfault issue in LPC55S69.

I have created a c++ project and implemented changes for my project. As part of it, I am making use of C++ STL library features.

Below is the code snippet,

 

I have an enum defined with few CMD codes,
typedef enum
{
CMD_INVALID = 0x9999,
CMD_0 = 0x0000,
CMD_1 = 0x0001,
CMD_2 = 0x0002,
CMD_3 = 0x0003,
CMD_4 = 0x0004,
CMD_5 = 0x0005,
CMD_6 = 0x0006,
CMD_7 = 0x0007,
CMD_8 = 0x0008,
CMD_9 = 0x0009,
}CMD_CODES;

I have initialized the map container
std::map<std::string, CMD_CODES> Protocol::commands_map;

In an initialization routine, inserting the elements
commands_map.emplace( std::string( "CMD1" ), CMD_1);
commands_map.emplace( std::string( "CMD2" ), CMD_2 );
commands_map.emplace( std::string( "CMD3" ), CMD_3 );
commands_map.emplace( std::string( "CMD4" ), CMD_4 );
commands_map.emplace( std::string( "CMD5" ), CMD_5 );
commands_map.emplace( std::string( "CMD6" ), CMD_6 );
commands_map.emplace( std::string( "CMD7" ), CMD_7 );
commands_map.emplace( std::string( "CMD8" ), CMD_8 );
commands_map.emplace( std::string( "CMD9" ), CMD_9 );

 

 

After this initialization, I will performing other tasks.

But I am getting a hardfault error, in the initialization routine while inserting the elements. I am wondering, what is going on here.

sushmasan_0-1724791519409.png

Can someone please let me know, what the issue is?

 

Regards,

San

0 Kudos
Reply
1 Solution
3,527 Views
ErichStyger
Specialist I

Hi @sushmasan ,

both heap and stack (MSP) size you can easily change in the linker settings in MCUXpresso IDE (no linker file modification needed). Here are the settings with the MPS stack marked:

ErichStyger_0-1725017655568.png

 

As for PSP (process stack pointer): this is used for the stacks of threads. Settings is depending on the RTOS used, for example for FreeRTOS it is a configuration define:

#define configTOTAL_HEAP_SIZE                       (32*1024)

I hope this helps,

Erich

View solution in original post

6 Replies
3,509 Views
sushmasan
Contributor II

Thanks for explanation @ErichStyger , @Harry_Zhang, it is very helpful.

0 Kudos
Reply
3,581 Views
sushmasan
Contributor II

While debugging the code, what I noticed was the heap size increasing which is very close to 100%, that's when hardfault is triggered. When I checked the allocated stack and heap size it was 4KB, that was the reason for the failure. After configuring the heap size to 8KB, the code worked just fine. The heap size used was around 6.2KB.

As you mentioned try more space for MSP, PSP stack. How can I do that?

0 Kudos
Reply
3,527 Views
ErichStyger
Specialist I

Hi @sushmasan ,

both heap and stack (MSP) size you can easily change in the linker settings in MCUXpresso IDE (no linker file modification needed). Here are the settings with the MPS stack marked:

ErichStyger_0-1725017655568.png

 

As for PSP (process stack pointer): this is used for the stacks of threads. Settings is depending on the RTOS used, for example for FreeRTOS it is a configuration define:

#define configTOTAL_HEAP_SIZE                       (32*1024)

I hope this helps,

Erich

3,525 Views
ErichStyger
Specialist I

to add to that: the stack size for each task in FreeRTOS is assigned as parameter in the xTaskCreate() API call.

0 Kudos
Reply
3,540 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @sushmasan 

To increase the stack sizes for the Main Stack Pointer (MSP) and the Process Stack Pointer (PSP) in an MCUXpresso project, you typically need to modify the linker script or relevant configuration settings in your project. Here’s how you can do that:

1. Check the Heap Size Definition
If you need to modify the heap size as well, look for similar definitions for the heap:
__HeapBase = __end__;
__HeapLimit = __StackLimit;
The heap size is usually defined by the difference between __HeapBase and __HeapLimit. Adjust these definitions accordingly if needed.
2. Adjusting MSP and PSP Stack Sizes
The MSP is used by default and typically allocated from the top of the RAM. If you are using a Real-Time Operating System (RTOS) like FreeRTOS, the PSP is used for tasks, and its size is managed by the RTOS configuration. For bare-metal applications, MSP adjustments in the linker script are usually sufficient.

For RTOS-based applications:

• MSP Stack Size: Controlled by the linker script (as shown above).
• PSP Stack Size: Adjusted via the RTOS configuration, often defined in FreeRTOSConfig.h or a similar configuration file.

BR

Hang

3,586 Views
ErichStyger
Specialist I

Looks like a possible stack overflow to me. Try to reserve more space for your MSP and PSP stack.

Other than that: this is the hardfault handler I'm using:
https://github.com/ErichStyger/McuOnEclipseLibrary/blob/master/lib/src/McuHardFault.c

I hope this helps,

Erich

0 Kudos
Reply