GPIO Interrupts on LPC546xx

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GPIO Interrupts on LPC546xx

1,235 次查看
andyjackson
Contributor III

Looking at the latest LPC546xx datasheet (2.6) it says in section 7.15.1 GPIO Features that:

* All GPIO pins can be selected to create an edge or level-sensitive GPIO interrupt request

I need to get an interrupt from pin P4.7 but I cannot see how to achieve this. Both the PINT and GINT blocks only appear to function on GPIO ports 0 or 1 and I can't see any interrupt function in the GPIO block.

I'm clearly missing something as the datasheet is quite clear that all GPIO pins can generate an interrupt.

Thanks for any help,

Andy

标签 (2)
标记 (1)
0 项奖励
回复
1 回复

1,112 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Andy Jackson ,

The P4.7  cannot generate interrupt , both PINT and GINT cannot support it.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复