FreeRTOS+IO with LPC11UXX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FreeRTOS+IO with LPC11UXX

675 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by neilt6 on Thu Jul 25 15:12:11 MST 2013
Just wondering if anybody's had success marrying the LPCOpen LPC11UXX chip drivers with FreeRTOS+IO? I skimmed through the demo project for the LPC17XX chips, but the BSP layer is dauntingly complicated. Without other examples to compare against, I'm not really sure where to start porting...
标签 (1)
0 项奖励
回复
1 回复

661 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Thu Aug 15 09:59:48 MST 2013
There is a FreeRTOS example for the LPC11Uxx included in LPCOpen.
You can find it in the following LPCOpen directory:  LPCOpen\lpcopen_v1.03\applications\lpc11xx\xpresso_projects\nxp_xpresso_11u14
Look at the "nxp_xpresso_11u14_freertos_blinky" example.
0 项奖励
回复