Hello dear NXP community, I would like to flash a bootloader on a LPC5410x with the mxli-3.3 tool from marc. The processor is recognised with the command ./mxli -n and output in the command line.
When trying to load a hex file onto the board, the error: Segmentation fault. I have read that errors can occur with hex files. So I tried to load a binary file. With the windows tool flash magic the loading worked without problems.
I tried to display some error causes with the following command:
./mxli -q -d/dev/ttyUSB0 -b115200 -c12M -g -v -k -i -x -E -T 10000 -p -G 3 LCS_Bootloader_Release.bin
The first partitions of the RAM were also successfully written:
Download to RAM [4096@0x02000000...
Download to RAM [4096@0x02001000...
Download to RAM [4096@0x02002000...
However, with RAM [4096@0x02003000... the errors came up:
ERROR: Data expected from LPC
ERROR: binary echo mismatch.
ERROR: write FLASH failed
Could someone perhaps give me a push in the right direction with this problem, or help me to find out where the problem is? I am grateful for any answer and help