Field Oriented Control (FOC) of PMSM motor using LPC15xx

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Field Oriented Control (FOC) of PMSM motor using LPC15xx

1,037 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rces on Tue Apr 26 09:24:28 MST 2016
Hi all members,
we own a "OM13067: LPC1549 Motor Control Kit"  and we can successfully send command to and get status from the evaluation board using firmware demo either via GUI or via text console.
FOC works as expected with Teknic motor but... we can't understand why in the firmware and also in the AN11517 application note (precisely at pages 15/39 and at pages 16/39) there is  a swap between d-axis and q.axis (please look at figures 11 and 13).
I mean: with FOC conditions fullfilled, d-axis PI regulator output should set PMSMS flux reference (Vd reference) and q-axis PI regulator output should set PMSM torque reference (Vq reference) as figure 13 tries to explain.
Figure 11, on the other hand,  states that Idset (instead of Iqset!!!) comes from speed output regulator.

Maybe we miss something...

Thank you in advance for any help.

rces
标签 (1)
0 项奖励
回复
1 回复

910 次查看
lpcware
NXP Employee
NXP Employee
bump
0 项奖励
回复