External Trigger to HSADC using SGPIO10

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

External Trigger to HSADC using SGPIO10

1,590 次查看
shivam0078
Contributor I

Kindly suggest a way to trigger HSADC of LPC 4370 using SGPIO10. If possible then please send the snippet of the code as well. @ravithakur 

标签 (3)
0 项奖励
回复
2 回复数

1,582 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

we do not know what logic of SGPIO you would like to implement, anyway, I think an11275.zip is helpful for your understanding SGPIO module, pls refer to it.

Hope it can help you

https://www.nxp.com.cn/docs/en/application-note/AN11275.zip

 

BR

XiangJun Rong

0 项奖励
回复

1,515 次查看
shivam0078
Contributor I

Thanks for your reply. I want a trigger pin using which I can trigger the hsadc externally in lpc link 2 board. From the datasheet I have found that I can trigger the hsadc using SGPIO10. I have configured the sgpio10 to the P1_3 pin of LPC4370 controller. Then I have connected the SGPIO10 as a trigger to HSADC using GIMA. Please suggest me a way to trigger HSADC externally.

 

0 项奖励
回复