Ethernet interrupt lockup, caused by mysterious "reserved" MAC interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet interrupt lockup, caused by mysterious "reserved" MAC interrupt

717 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larsjep on Tue Jan 14 01:26:56 MST 2014
Hi,

I have a problem with the Ethernet controller when using a DP83620SQ Phy.
This Phy should be more or less compatible with the the DP8384 on the Hitex eval board.

The problem is that sometimes at startup I keep getting ethernet interrupt.
If I check the DMA_STAT register none of the interrupt bits is set.
But if I check MAC_INTR bit 10 it set, when the problem occurs ??
According to the manual this bit is just "reserved"

This bit get set right after I send a reset command to the Phy. (But only sometimes)

What is the meaing of this bit 10 in the MAC_INTR register ?
And why does it get set ?

Best regards
  Lars
Labels (1)
0 Kudos
Reply
0 Replies