Errata of LPC43xx vs LPC43Sxx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Errata of LPC43xx vs LPC43Sxx

Jump to solution
576 Views
johanborkhuis
Contributor III

According to the errata sheet of the LPC435x there is an issue with the CAN registers when using in combination with the ADC and other per (see C_CAN.1 in the errata sheet). However, this issue is not shown in the the errata sheet of the LPC43S5x. Is this problem solved in the LPC43S5x?

Or, to rephrase it more general: does the errata sheet of the LPC435x also apply to the LPC43S5x?

Regards,

Johan

Labels (1)
1 Solution
424 Views
soledad
NXP Employee
NXP Employee

Hi,

The C_CAN.1 errata doesn't apply for LPC43S37JET100; LPC43S57JET256; LPC43S37JBD144; LPC43S57JBD208 devices,

The C_CAN.1 errta applies for the below devices:

LPC4370FET100; LPC4370FET256; LPC4350FET256; LPC4350FET180; LPC4330FET256; LPC4330FET180; LPC4330FET100; LPC4330FBD144; LPC4320FET100; LPC4320FBD144; LPC4310FET100; LPC4310FBD144

Revisions A, C and D.

In additon: LPC4357FET256; LPC4357JET256; LPC4357JBD208; LPC4353FET256; LPC4353JET256; LPC4353JBD208; LPC4337FET256; LPC4337JET256; LPC4337JBD144; LPC4337JET100; LPC4333FET256; LPC4333JET256; LPC4333JBD144; LPC4333JET100; LPC4327JBD144; LPC4327JET100; LPC4325JBD144; LPC4325JET100; LPC4323JBD144; LPC4323JET100; LPC4322JBD144; LPC4322JET100; LPC4317JBD144; LPC4317JET100; LPC4315JBD144; LPC4315JET100; LPC4313JBD144; LPC4313JET100; LPC4312JBD144; LPC4312JET100

only for Initial device revision.

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
425 Views
soledad
NXP Employee
NXP Employee

Hi,

The C_CAN.1 errata doesn't apply for LPC43S37JET100; LPC43S57JET256; LPC43S37JBD144; LPC43S57JBD208 devices,

The C_CAN.1 errta applies for the below devices:

LPC4370FET100; LPC4370FET256; LPC4350FET256; LPC4350FET180; LPC4330FET256; LPC4330FET180; LPC4330FET100; LPC4330FBD144; LPC4320FET100; LPC4320FBD144; LPC4310FET100; LPC4310FBD144

Revisions A, C and D.

In additon: LPC4357FET256; LPC4357JET256; LPC4357JBD208; LPC4353FET256; LPC4353JET256; LPC4353JBD208; LPC4337FET256; LPC4337JET256; LPC4337JBD144; LPC4337JET100; LPC4333FET256; LPC4333JET256; LPC4333JBD144; LPC4333JET100; LPC4327JBD144; LPC4327JET100; LPC4325JBD144; LPC4325JET100; LPC4323JBD144; LPC4323JET100; LPC4322JBD144; LPC4322JET100; LPC4317JBD144; LPC4317JET100; LPC4315JBD144; LPC4315JET100; LPC4313JBD144; LPC4313JET100; LPC4312JBD144; LPC4312JET100

only for Initial device revision.

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------