Emwin NOT working properly with SSD 1963 in 8 bit mode.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Emwin NOT working properly with SSD 1963 in 8 bit mode.

780 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by AkshayHV on Sat Oct 26 06:44:14 MST 2013
Hi i am interfacing a 4.3 inch TFT with LPC1768 ,the controller in the display is SSD1963
it is basically a parallel 8 bit interface but the problem is even though the interface is of 8 bit in the SSD_init() function if i am sending a command to say it is 8 bit interface my display is not working properly but if i configure it as 9 bit interface it is working for some of the GUI in emwin but for some GUI's the colors are not displaying as normal



thanks and regards
Akshay H V
Labels (1)
0 Kudos
Reply
1 Reply

674 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Wouter on Tue Oct 29 08:00:14 MST 2013
Hi Akshay,

I just responded to your other thread (http://www.lpcware.com/content/forum/can-we-configure-emwin-16-bit-data-transfer-our-8-bit-data-line...). In the future please try avoid opening multiply threads on the same subject.

By the looks of your code, the low-level routines are not according to spec, and the 18bpp mode you selected in the init functions is not supported by the emWin driver. If you fix those two issues, you just might be lucky and have a working LCD.

Regards,
Wouter
0 Kudos
Reply