Does the MCUxpresso software v10.1.0. works with the ROBOVERO board from gumstix?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does the MCUxpresso software v10.1.0. works with the ROBOVERO board from gumstix?

880件の閲覧回数
jbenitezbasante
Contributor I

hello everybody! I am using Robovero board where  has a microcontroller LPC1769 I would like to know if it works with MCUxpresso software I want to try to flash program on board this is the posible?

thank you

ラベル(1)
0 件の賞賛
返信
1 返信

808件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

MCUXpresso supports the LPC1769 but no the RoboVero board.

You can use the JTAG for programming and debugging the LPC1769 using MCUXpresso.

GUMSTIX suggests to manage the Cortex-M3 from the onboard Overo COM or from an external USB interface using our very own HUBCOMMANDER interface.

https://s3-us-west-2.amazonaws.com/media.gumstix.com/datasheets/PKG30019.pdf 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信