Does W25Q32 is in support list of QSPI Flash.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does W25Q32 is in support list of QSPI Flash.

1,018件の閲覧回数
li-chinwang
Contributor II

LPC1830 use S25FL032P0XMFI013 as a QSPI Boot Device.

If customer want to use W25Q32 to replace S25FL032P0XMFI013 for cost down, does W25Q32 is in support list of QSPI  Flash.

I see some 3 party LPC1830 EVB use W25Q32 as boot QSPI Flash Device. 

ラベル(1)
0 件の賞賛
返信
1 返信

878件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Li-Chin Wang,

  Please check this picture:

pastedImage_1.png

W25Q32 already in the supported list, so you can use it!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信