Does LPC54114 audio and voice recognition kit has capability of Echo cancellation and noise cancellation?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does LPC54114 audio and voice recognition kit has capability of Echo cancellation and noise cancellation?

1,040 Views
kamalakannanr
Contributor I

Hi,

Does LPC54114 audio and voice recognition kit has capability of Echo cancellation and noise cancellation?

0 Kudos
Reply
2 Replies

854 Views
soledad
NXP Employee
NXP Employee

Hello,

 

Unfortunately the LPC54114 audio and voice recognition kit doesn’t has these capabilities implemented. The application note AN11855 explains the advantages of the LPC5411x ARM Cortex-M4F microcontroller family for a product which requires voice detection and voice recognition features.

http://cache.nxp.com/documents/application_note/AN11855.zip


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

854 Views
brendonslade
NXP TechSupport
NXP TechSupport

The LPC54114 has a Cortex M4F, so is certainly capable of performing some of these functions (depending on the requirements of the particular algorithms used), but NXP does not currently have a partner offering this software.

0 Kudos
Reply