Diference Between LPC1768FBD100,551 and LPC1768FBD100K

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Diference Between LPC1768FBD100,551 and LPC1768FBD100K

Jump to solution
1,138 Views
contr2889
Contributor III

Hi everyone,

    I hope you have a nice day. I was searching for LPC1768FBD100,551 and I just noticed that this component is obsolete, but could be remplaced by LPC1768FBD100K. My question is, Is there any difference between these chips? Are them compatible pin to pin? I was looking this information in datasheet but is a little confused for me. Thanks for your help.

Best Regards

Labels (1)
0 Kudos
1 Solution
1,128 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Tomas,

Regarding the difference Between LPC1768FBD100,551 and LPC1768FBD100K, pls refer to the following link:

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

For the LPC1768FBD100,551 and LPC1768FBD100K, the processor is same from package, pin assignment, feature, function...

The only difference is the Packing: TRAY-Tray, for the LPC1768FBD100,551, the tray is with Package Quantity: 90.   For the LPC1768FBD100K, the tray is with Package Quantity: 450.

Hope it can help you

BR

XiangJun rong

 

View solution in original post

0 Kudos
2 Replies
1,129 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Tomas,

Regarding the difference Between LPC1768FBD100,551 and LPC1768FBD100K, pls refer to the following link:

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

For the LPC1768FBD100,551 and LPC1768FBD100K, the processor is same from package, pin assignment, feature, function...

The only difference is the Packing: TRAY-Tray, for the LPC1768FBD100,551, the tray is with Package Quantity: 90.   For the LPC1768FBD100K, the tray is with Package Quantity: 450.

Hope it can help you

BR

XiangJun rong

 

0 Kudos
1,111 Views
contr2889
Contributor III

@xiangjun_rongThanks for your reply

0 Kudos