Hi everyone,
I hope you have a nice day. I was searching for LPC1768FBD100,551 and I just noticed that this component is obsolete, but could be remplaced by LPC1768FBD100K. My question is, Is there any difference between these chips? Are them compatible pin to pin? I was looking this information in datasheet but is a little confused for me. Thanks for your help.
Best Regards
Solved! Go to Solution.
Hi, Tomas,
Regarding the difference Between LPC1768FBD100,551 and LPC1768FBD100K, pls refer to the following link:
For the LPC1768FBD100,551 and LPC1768FBD100K, the processor is same from package, pin assignment, feature, function...
The only difference is the Packing: TRAY-Tray, for the LPC1768FBD100,551, the tray is with Package Quantity: 90. For the LPC1768FBD100K, the tray is with Package Quantity: 450.
Hope it can help you
BR
XiangJun rong
Hi, Tomas,
Regarding the difference Between LPC1768FBD100,551 and LPC1768FBD100K, pls refer to the following link:
For the LPC1768FBD100,551 and LPC1768FBD100K, the processor is same from package, pin assignment, feature, function...
The only difference is the Packing: TRAY-Tray, for the LPC1768FBD100,551, the tray is with Package Quantity: 90. For the LPC1768FBD100K, the tray is with Package Quantity: 450.
Hope it can help you
BR
XiangJun rong
@xiangjun_rongThanks for your reply