Data rate of LPC4300 USB mass storage host with USB pendrives (USB 2.0 and 3.0)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Data rate of LPC4300 USB mass storage host with USB pendrives (USB 2.0 and 3.0)?

589件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Prithvi on Fri Dec 06 19:19:28 MST 2013
Hi all,
I am looking for a storage solution for a camera application with LPC4300. The storage should be high speed (>25 MBps) and have high capacity (minimum 2 GB). Ability to swap (SD card or pendrive) is a plus.
SD card might not be a solution since UHS-1 standard (DDR50 mode) is not supported. USB 2.0 pendrives are not fast enough. But the recent USB 3.0 pen drives are fast and also backward compatible with USB 2.0 and might be able to give a data rate of 25 MBps with a USB 2.0 HS port (sequential write). Anyone tested this? What is the maximum data rate achieved with USB Mass storage in host mode with LPC4300?
Thanks a lot!
ラベル(1)
0 件の賞賛
返信
0 返答(返信)