DMA transfer from register PIN0 or MPIN0 to RAM on 824 chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DMA transfer from register PIN0 or MPIN0 to RAM on 824 chip

776 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ntil on Sun May 08 04:42:05 MST 2016
Good day all.
Can DMA make transfers from PIN0 or MPIN0 registers to SRAM on 824 chip ?
When I try it, i got DMA error.
Other memory-to-memory or UART-to-memory transfers works fine..
It looks like not allowed to transfer with DMA from any register? only specific (SPI,UART, etc)..
but "LPC82x User manual" tells "The source and destination end addresses, as well as the link to the next descriptor are
just memory addresses that can point to any valid address on the device."
So can I read with DMA any register or only specific?
Thanks.
Labels (1)
0 Kudos
Reply
1 Reply

685 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply