DMA transfer from register PIN0 or MPIN0 to RAM on 824 chip

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DMA transfer from register PIN0 or MPIN0 to RAM on 824 chip

514件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ntil on Sun May 08 04:42:05 MST 2016
Good day all.
Can DMA make transfers from PIN0 or MPIN0 registers to SRAM on 824 chip ?
When I try it, i got DMA error.
Other memory-to-memory or UART-to-memory transfers works fine..
It looks like not allowed to transfer with DMA from any register? only specific (SPI,UART, etc)..
but "LPC82x User manual" tells "The source and destination end addresses, as well as the link to the next descriptor are
just memory addresses that can point to any valid address on the device."
So can I read with DMA any register or only specific?
Thanks.
ラベル(1)
0 件の賞賛
返信
1 返信

423件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信