Controlling of Servo Motor Using LPC11C24

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Controlling of Servo Motor Using LPC11C24

785件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mahalinr on Sat Oct 18 08:09:52 MST 2014
I am having an FS90R Continous Servo Motor with 3 wires.

1.Vss 5V

2.PWM Signal

3. Gnd

I have already initalized the PWM Signal through 16bit Timer Function from LPC11C24 Sample Program.

My PWM Port is PIO1_10/AD6/CT16B1_MAT1.. For further reference plz see the attached program

Can anyone tell me how to control this Servo Motor after Initalizing this PWM Signal.

Thanks

Original Attachment has been moved to: timer16_1.c.zip

ラベル(1)
0 件の賞賛
返信
0 返答(返信)