Configuration of RGB lcd (40 pin) and LPC1788

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configuration of RGB lcd (40 pin) and LPC1788

1,285件の閲覧回数
miladcalipa
Contributor I

I,m beginner in ARM and need help about configuring RGB LCD with lpc1788 build-in LCD controller in MDK-5.  If somebody tell me about or give me really easy example with emwin,  I will be so greatful

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,001件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please check the AN11244 application note. This application note describes the basics of using emWin on NXP microcontrollers. Please let me know if this helps.

http://www.nxp.com/documents/application_note/AN11244.pdf 

emWin Graphics Library|NXP 

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信