Concerning the ADC of the LPC1549JBD64: Is it possible to measure an analog voltage on ADC0_1 and ADC1_0 simultaneously, or can it only be done sequentially?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Concerning the ADC of the LPC1549JBD64: Is it possible to measure an analog voltage on ADC0_1 and ADC1_0 simultaneously, or can it only be done sequentially?

796 次查看
maxveen
Contributor I

Simultaneous measurements on ADCchannels of LPC1549 

0 项奖励
回复
1 回复

680 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Max Veen,

Thank you for your interest in NXP Semiconductor products and  the opportunity to serve you.Is 

it possible to measure an analog voltage on ADC0_1 and ADC1_0 simultaneously, or can it only be done sequentially?
--- Yes, they can sample the signals simultaneously.

Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复