Code protection on FLASH-less parts

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Code protection on FLASH-less parts

706 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lbodnar on Sat Feb 16 07:14:18 MST 2013
Hi,

I have not used LPC43xx series before.
Most of the LPC43xx in TQFP packages are sold as FLASH-less parts.
If I were to use this in a product, how the code protection is ensured?

Thanks
Leo
标签 (1)
0 项奖励
回复
2 回复数

672 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lbodnar on Tue Feb 19 01:12:32 MST 2013
Thanks Dave,

Where can I buy flash versions of LPC43xx in production qty? 

No distributor carries a stock of TQFP parts with flash.

I used to work with Microchip products and you typically get them in 100's qty from online distributors (Digikey/Farnell/Mouser/Arrow) and from Microchip online store if you need 1000's+.
You can always find some stock somewhere if you are caught short.

I'd like to have a go at NXP parts but how do I source the parts?

Thanks
Leo
0 项奖励
回复

672 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxp21346 on Mon Feb 18 15:26:41 MST 2013
NXP's feature "Code Read Protection" is implemented on NXP parts with on-chip flash. The LPC43xx variants without on-chip flash don't implement CRP. It would be harder to secure code on a flashless part that boots and runs from external memory.

-Dave @ NXP
0 项奖励
回复