Changing baud rate of LPC 4370

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Changing baud rate of LPC 4370

878 Views
vxs187
Contributor III

I don't know how to change the UART's baudrate for an LPC4370 microcontroller. I am using an example program from LPCExpresso to change the baudrate, from the board.c file. It has a function as follows:

Chip_UART_SetBaud(DEBUG_UART, 115200);

I have also included the function definition below:

uint32_t Chip_UART_SetBaud(LPC_USART_T *pUART, uint32_t baudrate)
{
uint32_t div, divh, divl, clkin;

/* Determine UART clock in rate without FDR */
clkin = Chip_Clock_GetRate(Chip_UART_GetClockIndex(pUART));
div = clkin / (baudrate * 16);

/* High and low halves of the divider */
divh = div / 256;
divl = div - (divh * 256);

Chip_UART_EnableDivisorAccess(pUART);
Chip_UART_SetDivisorLatches(pUART, divl, divh);
Chip_UART_DisableDivisorAccess(pUART);

/* Fractional FDR alreadt setup for 1 in UART init */

return clkin / div;
}

As seen, the baud rate is set by dividing the clkin by div. I am trying to achieve a baud rate higher than 115200, and it doesn't really work as it does for transferring data serially to an Arduino, as it does at 115200. I am new to using the microcontroller, any help would be greatly appreciated. 

Thanks!

Labels (1)
0 Kudos
1 Reply

744 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Visweshwar Srinivasan,

Please refer to the formula that is shown in the user guide section 40.6.12 to see which is the maximum baud rate you can reach depending on the peripheral clock. 

pastedImage_1.png

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos