Change PHY to DP83848 in LWIP_lpc-v08.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Change PHY to DP83848 in LWIP_lpc-v08.0

2,724 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by karakas on Fri Sep 25 06:09:47 MST 2015
Hi dear
I have my own LPC1788 Board and I want to launch Ethernet by LWIP LPC.
I downloaded LWIP_lpc-v08.0 and without any change programed to MCU and that works and I have ping.
After that I found PHY library in program is LAN8720 but my PHY is DP83848 but I didn't know how it works?!
However,I change PHY configuration for DP83848 According to LWIP Doc.but it doesn't work and there isn't any ping.
How should I configure PHY in LWIP_lpc-v08.0?
Is there more configuration than Doc.?

thanks
Labels (1)
0 Kudos
Reply
3 Replies

2,076 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Gbrus on Tue Sep 29 01:28:13 MST 2015
I use the same PHY on a custom board. I replaced the LAN8720 driver in the board library with the driver attached.
0 Kudos
Reply

2,076 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Sun Sep 27 20:35:31 MST 2015
I think that the original example download (from the EA site) for the 1778 baseboard etc.
had the DPxxx PHY instead of a LAN8720.

And possibly the old NXP easy web example too.

HTH, Mike.
0 Kudos
Reply

2,076 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by karakas on Sun Sep 27 11:10:10 MST 2015
How can I configure PHY in LWIP_lpc-v08.0 to DP83848?
0 Kudos
Reply