Cant program flash or debug

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Cant program flash or debug

1,998 次查看
johnnifriis
Contributor I

LPC1837JET256, chip rev.'A', I'm using Keil and ulink2 (SWD) on our hardware. I can not download to flash.

I get errors like: "Could not stop Cortex M device".

I have verified signals in the debug connector. Pin10 was not reset, it has been changed.  

Got 10K pullup on SWDIO, SW0, TDI, 10k pulldown on SWDCLK. and TRST is floating.

Reset is 10k pullup and 100nF to GND, and a switch to GND.

I checked DBGEN, it is at 3.3V.

ISP (P2_7 - A9 in my case) is at 3,3V during reset and else at 0,3V. See below too.

If I remove the reset signal, I can program flash and the 6 LED blinks as expected. Something is working....

I have compared the debug interface on my board with the MCB1800 EV-board and it seems to be identical.

If I switch to MCB1800 (LPC1857JET256, chip rev '-') I can program and debug, so the ulink2 seems to work, project settings seems to be ok. There must be some kind of difference between the two.

If I set ISP low (by a DIP switch) and toggels reset, no LEDs are blinking - it is in ISP mode. If I set DIP sw off and toggles reset the LEDs starts blinking - program running. So the ISP seems to be ok. I wonder why it is low after reset?

Attached first 3 pages of my diagram and a more detailed description in word.

Any ideas would be highly appreciated

标签 (2)
标记 (1)
0 项奖励
回复
1 回复

1,814 次查看
johnnifriis
Contributor I

I tried NXP expreso with NXP-link2, worked out the box.

It turned out there is an error in KEIL for the 18xx family. The feature can be disabled and it works....

I used uVision 5.21a, an update to 5.22 did not solve the issue. It will be solved in the next update - Keil support told me

To disable the feature, that is not working, go to:

Options for target -> Debug tap -> settings (for ULINK2) -> Pack: Remove the checkmark in 'enable'

0 项奖励
回复