Can we get project files of emwin graphics BSP with VC++6.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can we get project files of emwin graphics BSP with VC++6.0

713件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ravi Teja on Thu May 24 03:21:09 MST 2012
Hi

  Right now in emwin 5.14 BSP they have given VC++ files which will be supported in Visual studio 10.0 . But now i don't have that software. I have only visual studio 6.0 licenced version can we get the files which are supported int this version? Then how can we access or get these old versions of emwin grphics library.
ラベル(1)
0 件の賞賛
返信
1 返信

678件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by drs on Thu May 24 07:35:11 MST 2012
The old style VS 6.0 project files are in the v5.12 BSPs. I suggest you use these and update as needed to work with the v5.14 BSP.

The solution files in the v5.14 were tested with VS 2010 Express which is free.
0 件の賞賛
返信