Can USB1 in high speed mode working with 12MHz system clock in LPC55S28 controller?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can USB1 in high speed mode working with 12MHz system clock in LPC55S28 controller?

3,058 Views
rahulshah
Contributor I

Hi,

In our design it is required to use USB1 in high speed mode with 12MHz system clock.

So is USB1 in High-speed mode should work with 12MHz system clock? 12MHz system clock derived from FRO_12M.

Also in our design 12MHz crystal connected on XTAL32M for USB1-PHY clock.

So this solution should work or not? I have tested with different system clock as below and found following results.

 

system clockderived fromUSB1 High speed status
12 MHzFRO_12MNot working
16 MHzFRO_96MNot working
19.2 MHzFRO_96MNot working
24 MHzFRO_96MNot working
32 MHzFRO_96Mworking
48 MHzFRO_96Mworking
96 MHzFRO_96Mworking
150MHzPLL150Mworking
50MHzPLL150Mworking
37.5MHzPLL150Mworking
30MHzPLL150Mnot working

 

Regards,

Rahul Shah

Labels (1)
0 Kudos
Reply
2 Replies

3,041 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

USB1 must work with external crystal osc. internal osc is not for USB1.

see below:

Initial configuration of the USB1_PHY:
• Clocks:
– The XO32M crystal oscillator and must be powered up and configured to one of the
supported USB1_PHY reference clock frequencies of 16 MHz, 19.2 MHz, 20 MHz,
24 MHz or 32 MHz. Set the ENABLE_USB_HS_CLK_OUT bit of the
XO32M_CTRL register to enable the XO32M clock output to the USB1_PHY. See
Section 11.5.5.
– Enable the 32k_osc clock to provide the 32 kHz clock to the USB1_PHY.
– Set USB1_PHY in AHBCLKCTRL2, to enable clock to the USB1_PHY’s APB
register interface

 

Best Regards

Jun Zhang

0 Kudos
Reply

3,032 Views
rahulshah
Contributor I

Hi Jun Zhang,

Thanks for your reply.

So i have used and SDK example code "SDK_2.8.0_LPCXpresso55S28\boards\lpcxpresso55s28\usb_examples\usb_device_hid_generic\bm".

In that default system clock is 150MHz, and with LPC55S28 EVM kit USB1 as high speed works fine with above example code. 

Now if i change system clock to 12MHZ by using "BOARD_BootClockFRO12M" function in above example code, then USB1 as High-speed not working.

Note : with both usecase (12MHz and 150MHz system clock)16MHz crystal is connected to "XTAL32M" and USB1_PHY takes clock from that crystal.

Please find clock configuration image for 12MHz and 150MHz .

Regards,

Rahul Shah

0 Kudos
Reply