Can LPC546x's SPIF connect to serial SRAM that supports QSPI?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can LPC546x's SPIF connect to serial SRAM that supports QSPI?

634 Views
geweilin
Contributor II

Since the SPIF can support QSPI interface flash, I wonder this interface can support QSPI SRAM?

Labels (2)
0 Kudos
Reply
1 Reply

557 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Yes, I think so.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply