Can LPC2478FET208,551 replace a LPC2470FET208,551 design?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can LPC2478FET208,551 replace a LPC2470FET208,551 design?

604件の閲覧回数
jetbig
Contributor I

The LPC2470 has no flash.  Wanted to know if the LPC2478 can drop in replace the LPC2470 and not use its on board flash?  Is there something special we need to do with the LPC2478 to get it to not use its onboard flash?

0 件の賞賛
返信
3 返答(返信)

592件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

LPC2470 is flashless version of LPC2478. they are pin to pin replacement.

theoretically, you use LPC2470 project directly on LPC2478. 

0 件の賞賛
返信

588件の閲覧回数
jetbig
Contributor I

So are you saying that an unprogrammed LPC2478 will automatically act like a flashless LPC2470 and directly load the external program without any special configuration?

0 件の賞賛
返信

583件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

yes, just make sure your LPC2478 board has the same PCB design as LPC2470.

LPC2470 project can work on LPC2478 directly.

 

0 件の賞賛
返信