Can LPC2478FET208,551 replace a LPC2470FET208,551 design?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can LPC2478FET208,551 replace a LPC2470FET208,551 design?

604 Views
jetbig
Contributor I

The LPC2470 has no flash.  Wanted to know if the LPC2478 can drop in replace the LPC2470 and not use its on board flash?  Is there something special we need to do with the LPC2478 to get it to not use its onboard flash?

0 Kudos
Reply
3 Replies

592 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

LPC2470 is flashless version of LPC2478. they are pin to pin replacement.

theoretically, you use LPC2470 project directly on LPC2478. 

0 Kudos
Reply

588 Views
jetbig
Contributor I

So are you saying that an unprogrammed LPC2478 will automatically act like a flashless LPC2470 and directly load the external program without any special configuration?

0 Kudos
Reply

583 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

yes, just make sure your LPC2478 board has the same PCB design as LPC2470.

LPC2470 project can work on LPC2478 directly.

 

0 Kudos
Reply