Can I only use the M0 core with LPC54114?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I only use the M0 core with LPC54114?

1,056件の閲覧回数
da_chen
Contributor II

I found many examples about how to use dual cores. But no one said how to only use the M0 core to work. Is this possible?

ラベル(1)
タグ(2)
1 返信

955件の閲覧回数
brendonslade
NXP TechSupport
NXP TechSupport

The LPC5411x is intended for the M4 to release the M0+ since the M0+ is primarily there as a slave core, so the examples are geared up for this.

If you are looking for an M0+ only device with the same / very similar peripherals I'd suggest using the LPC51U68, which is a lower cost.