Can I Put 256MB SDRAM instead of 128MB in DYCS0?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I Put 256MB SDRAM instead of 128MB in DYCS0?

3,444 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by h.lotfi on Tue Dec 23 09:31:06 MST 2014
Hi,
i made a custom board with LPC4357.
i use section 128 MB dynamic external memory DYCS0 on memory map, but i put a 256MB SDRAM on board, (because i didn't know this section don't support 256MB SDRAM).
can i use 128MB of this SDRAM in this mode?
i test it but i can use just a few size of it...
i use this SDRAM: K4S561632C-TC75
Labels (1)
0 Kudos
Reply
6 Replies

3,391 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by emh203 on Fri Jan 30 12:05:18 MST 2015
I can verify that a IS42S32160D-7BLI-TR (512Megabit / 64 Megabyte)  works just fine at 102MHz clock.

0 Kudos
Reply

3,391 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by h.lotfi on Wed Jan 07 09:37:51 MST 2015

Quote: bavarian
Don't mix up Bits and Bytes  ;-)

DYCS0 supports an address range of 128MBytes, this means that you could have a 1Gbit SDRAM device.
But this range is not supported by the SDRAM controller, for a 16-bit SDRAM the MCU supports up to 512Mbit (= 64MByte) on each CS.

So don't worry, your 256Mbit SDRAM will work.

Regards,
NXP Support Team



Thank you very much  ;-)
0 Kudos
Reply

3,391 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Wed Jan 07 07:50:04 MST 2015
Don't mix up Bits and Bytes  ;-)

DYCS0 supports an address range of 128MBytes, this means that you could have a 1Gbit SDRAM device.
But this range is not supported by the SDRAM controller, for a 16-bit SDRAM the MCU supports up to 512Mbit (= 64MByte) on each CS.

So don't worry, your 256Mbit SDRAM will work.

Regards,
NXP Support Team
0 Kudos
Reply

3,388 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by h.lotfi on Sun Dec 28 06:57:26 MST 2014
Hi, I use this SDRAM: K4S561632C-TC75
it is 256Mb, but i put it on DYCS0 that it support 128Mb...
this SDRAM have same footprint and pinout with this SDRAM: K4S281632K that it is 128Mb...
i want know that is possible i put 256Mb on DYCS0 , but use of 128Mb or it is impossible?
0 Kudos
Reply

3,388 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Sat Dec 27 17:55:20 MST 2014
If it is a TSOP part, don't they have the same footprint/pinout?
So ... Just replace the chip.
0 Kudos
Reply

3,388 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by h.lotfi on Sat Dec 27 08:05:31 MST 2014
could any body help me?  :)
0 Kudos
Reply