CFAF320240F-035T and emwin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CFAF320240F-035T and emwin

980 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ali_asadzadeh on Mon Oct 10 03:05:45 MST 2011
Hi
I want to use the CFAF320240F-035T with SSD2119 controller and LPC1768 for the host mcu, along with the emWin library, but the library that you supplied does not contain the lcd derivers, Do you have any idea what I should do?
Regards
标签 (1)
0 项奖励
回复
1 回复

914 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ktownsend on Fri Oct 21 04:36:19 MST 2011
The only way to use the emWin library provided by NXP is with the LCD controller available on ,any of our higher-end ARM MCUs.  This may still work with certain LCDs with built in controllers, but the controller will need to be able to be configured to operate in the standard pixel clock format, effectively bypassing the LCD controller.  If you look at the Embedded Artists LPC1788 board and the 320x240 LCD this is exactly what they do.  They configure the LCD controller in the LCD to operate in pixel clock mode, and then drive the LCD directly with the LCD controller on the LPC1788.
0 项奖励
回复