Bug-fix for Hitex LPC4357 kit to make RMII autoconfigure correctly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bug-fix for Hitex LPC4357 kit to make RMII autoconfigure correctly

817件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rgledhill on Fri May 17 08:07:30 MST 2013

Hi,


There is a mistake on the Hitex LPC4357 kit where resistor R96 is 10k and needs to be 2k2.  This means that the auto-configure mode on the Ethernet PHY always defaults to MII mode, even if jumper JP5 is closed.


You can either change this resistor, or you can change your start-up code to force the PHY into RMII mode (if you want to use RMII mode!).  If you're using the Keil RTX TCPnet libraries, for instance, change ETH_LPC43xx.c:


:


:


            /* Configure the PHY device */
<strong>#if !_MII_ &amp;&amp; defined(HITEX_BOARD)</strong>
<strong>            write_PHY(PHY_REG_RBR, 0x20);   /* RMII mode - fix for Hitex LPC4357 board with inadequate config pull-up R96 */</strong>
<strong>#endif</strong>
#if defined(_10MBIT_)
:


:


 


This will be fixed in future revisions of the board; MII mode is unaffected.


Richard


Hitex UK Ltd

ラベル(1)
0 件の賞賛
返信
0 返答(返信)