Hello Team,
Actually i am trying to boot the LPC55S69 board through SD Card, i am not sure how much it is feasible.
If yes, any docs and pointer is really help me to move forward.
Actually i am exploring ways to boot the Board other than MCUXpresso IDE.
Another ways to boot is via a cmd line using JLinkGDBServer in that also one need to use external debugger to flash the program on to the board.
Is there a way to flash the application using internal debugger without the use of external hardware.
Any help is really appreciated!