Bit field descriptions for the Protected Flash Region

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Bit field descriptions for the Protected Flash Region

跳至解决方案
3,895 次查看
gvellet
Contributor II

Hi,

In the LPC55S69 user manual UM11126 page 252, it is written "Note: For bit field descriptions, see the attached Protected Flash Region.xls for further details."  Where can I find this excel file?

In the MCUXpresso Secure Provisioning tool, some information is given for the bitfield but it is not detailed.

For instance, in the location CMPA:SPI_FLASH_CFG, the bit field "SPI_RECOVERY_BOOT_EN" is 5-bit with no explanation. In the user manual, the same bitfield is said to have only 4-bit. Obviously the protected Flash bit fields are updated faster than the user manual.

Perhaps for designers with NXP device experience, most of these details are obvious. But for a new comer like me, I stumble a lot trying to understand this device.

Thanks

标签 (1)
0 项奖励
回复
1 解答
3,721 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @gvellet 

I'm sorry for the inconvenient to you. I have submitted request to add this.

I send you the Rev.2.5 for reference. Please see my attachment. Thanks.

 

BR

Alice

在原帖中查看解决方案

4 回复数
3,844 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @gvellet 

Please open the attachment in UM11126, you will find the "Protected Flash Region.xls". As below:

Alice_Yang_0-1719916196875.png

 

Please contact us if still have any issue.

 

BR

Alice

 

0 项奖励
回复
3,798 次查看
gvellet
Contributor II
The attachment is no longer in the latest PDF release. See my Tuesday july 2nd reply for details
0 项奖励
回复
3,722 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @gvellet 

I'm sorry for the inconvenient to you. I have submitted request to add this.

I send you the Rev.2.5 for reference. Please see my attachment. Thanks.

 

BR

Alice

3,833 次查看
gvellet
Contributor II

Hi Alice,

In the current UM11126 file, there is no attachment. Can you attached the xls file to this message thread?

gvellet_0-1719928129704.png

Thanks,

Gilbert Vellet

0 项奖励
回复