Bit band mapping on LPC5410x

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Bit band mapping on LPC5410x

跳至解决方案
1,475 次查看
rogerlittlewood
Contributor I

LPC5410x

There seems to be little info about using bit-banding on this device. Where can I find this information, for example mapping between the bit-band area and specific peripheral register bits? Which peripherals use bit-banding?......

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,277 次查看
ckphua
NXP Employee
NXP Employee

Hi,

LPC5410x User Manual did not describe this (and we will update in the next version). Meantime the LPC5410x Bit-band region is (0x4000 0000 to 0x40100000) can be accessed in the so-called alias region at 0x4200 0000.

This means all the APB Peripherals are mapped in the bit-band region.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,278 次查看
ckphua
NXP Employee
NXP Employee

Hi,

LPC5410x User Manual did not describe this (and we will update in the next version). Meantime the LPC5410x Bit-band region is (0x4000 0000 to 0x40100000) can be accessed in the so-called alias region at 0x4200 0000.

This means all the APB Peripherals are mapped in the bit-band region.

0 项奖励
回复
1,277 次查看
rogerlittlewood
Contributor I

Thanks. So I hope the new version comes out soon so we can start to use those clever features thoughtfully provided by the ARM system designers!

0 项奖励
回复